Welcome Aboard
https://uop.honeywell.com/en/search
Decoember 07, 2020

Tupraş Uses Honeywell Technology to Further Increase Diesel Fuel Production at Izmit Refinery 

Turkish refiner adds external heavy polynuclear aromatics stripper increasing hydrocracking unit conversion

DES PLAINES, III., Dec. 7, 2020 -- Honeywell today announced Turkiye Petrol Rafinerileri A.S. is improving the performance of its existing Honeywell UOP enhanced two-stage Unicracking™ process with the addition of an external heavy polynuclear aromatics (HPNA) stripper at its Izmit refinery. The HPNA stripper will enable Tüpraş to maximize conversion in the unit, increasing unit profitability through an increase in the yields of distillates and the flexibility to process heavier feedstocks.

UOP provided the basic engineering, catalysts and technical services for the project. UOP has more than 30 years’ experience in HPNA management and has commercially proven solutions for new units and existing units enabling customers to achieve near 100% conversion throughout the entire catalyst cycle life. The innovative HPNA side stripper technology applied at the Izmit refinery allows Tupras to carry out pioneering projects throughout its refinery sites and advance its production processes.

“UOP HPNA management solutions improve unit performance and profitability via increased conversion to high value products through enhanced catalyst performance due to slower catalyst deactivation,” said Bryan Glover, vice president and general manager, UOP’s Process Technologies business. “The external HPNA stripper increases the unit’s conversion efficiency by mechanically removing HPNAs that cause deactivation of the catalyst, and lets customers use heavier feedstocks.”

Since UOP's Unicracking process was introduced in 1960, the technology has advanced through the development of more effective catalysts, enhanced unit designs and novel reactor internals. Available in single- and two-stage processes, the technology is designed to produce higher yields of transportation fuels that adhere to tighter regulations using a wider range of feedstocks.

Honeywell UOP has licensed more than 240 Unicracking units in more than 50 countries. Including the Tüpraş unit at Izmit, UOP has licensed 19 enhanced two-stage Unicracking process units, with additional operating units in China and Turkey.

The Unicracking unit at Tüpraş is integrated with other UOP process technologies, including coker naphtha and distillate Unionfining™ units. The system, whose feedstocks include straight run diesel, coker gas oil and vacuum gas oils, was designed with a common fractionation section, reducing capital costs and improving Tüpraş' return on investment.

Tüpraş is the first producer in Turkey’s refining sector and the largest industrial enterprise of the country, operating four oil refineries with a total of 30 million tons annual crude oil processing capacity.

UOP LLC, a Honeywell company headquartered in Des Plaines, Illinois, is a leading international licensor of processing technology and supplier of engineering services, catalysts and adsorbents, equipment, specialty materials and digital solutions for the global refining, gas processing and petrochemical industries. With more than a century of leadership in hydrocarbon processing technologies, UOP has led six revolutions in technology that transformed the oil and gas industry. For more information visit www.uop.com.

Honeywell (www.honeywell.com) is a Fortune 100 technology company that delivers industry specific solutions that include aerospace products and services; control technologies for buildings and industry; and performance materials globally. Our technologies help everything from aircraft, buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable.  For more news and information on Honeywell, please visit www.honeywell.com/newsroom.

# # #

U.S. media contact:                                                                

Tehani Manochio                                                                      

(973) 216-0684                                                                        

tehani.manochio@honeywell.com

European media contact:

Martin Orsag

+4 2024 244 2279

martin.orsag@honeywell.com