November 02, 2021

Honeywell Introduces Revolutionary Plastics Recycling Technology to Drive A Circular  Plastics Economy

  • Honeywell’s UpCycle Process Technology expands the types of plastics that can be recycled
  • New technology can potentially increase the amount of global plastic waste that can be recycled to 90% when used in conjunction with other chemical and mechanical recycling processes
  • New technology can produce recycled feedstock used to make plastics with 57% less CO2-equivalent emissions than plastics produced from fossil feeds
  • Sacyr, a Spain-based engineering and services company, will be the first to use the technology

DES PLAINES, Ill., Nov. 2, 2021 – Honeywell (NASDAQ: HON) today announced the commercialization of a revolutionary process that expands the types of plastics that can be recycled and can produce feedstock used to make recycled plastics with a lower carbon footprint. The new technology can reduce the need for fossil fuels in the creation of virgin plastics while enabling hundreds of cycles of recycling, with the goal of enabling a circular economy for plastics.

Honeywell’s UpCycle Process Technology utilizes industry-leading molecular conversion, pyrolysis, and contaminants management technology to convert waste plastic back to Honeywell Recycled Polymer Feedstock, which is then used to create new plastics. The UpCycle Process technology expands the types of plastics that can be recycled to include waste plastic that would otherwise go unrecycled, including colored, flexible, multilayered packaging and polystyrene. When used in conjunction with other chemical and mechanical recycling processes -- along with improvements to collection and sorting – Honeywell’s UpCycle Process Technology has the potential to increase the amount of global plastic waste that can be recycled to 90%.

According to a study published by AMI International in September 2020, waste plastics processed through advanced recycling technologies, such as UpCycle Process Technology, could amount to between 5 and 15 million tons of additional plastic waste being recycled per year by 2030.1

Recycled plastics produced via UpCycle Process Technology can result in a 57% reduction of CO2-equivalent (CO2e) emissions compared with the production of the same amount of virgin plastic from fossil feeds.2. The process also reduces CO2e emissions by 77% compared with conventional modes of handling waste plastic, such as incineration and landfilling2. These CO2e reductions are some of the largest improvements among all pyrolysis technology offerings3, 4.

“Plastics play an important role in our society, including expanding the shelf life of food and making vehicles lighter, which reduces their emissions. Unfortunately, only a fraction of plastics today can be successfully recycled,” said Vimal Kapur, president and chief executive officer of Honeywell Performance Materials and Technologies. “Honeywell’s UpCycle process helps fix this problem. By broadening the types of plastic that can be recycled, UpCycle will revolutionize the plastics economy and play a critical role in improving the sustainability of many of the products we use on a daily basis.”

Sacyr, a Spain-based global engineering and services company with operations in more than 20 countries worldwide, will be the first to deploy Honeywell’s proprietary UpCycle Process Technology. Honeywell and Sacyr will form a joint venture where the two companies will co-own and operate a facility in Andalucía, in Southern Spain, with a capacity to transform 30,000 metric tons per year of mixed waste plastics into Honeywell Recycled Polymer Feedstock. Production is expected to begin in 2023.

Partnering with companies that have waste management experience such as Sacyr allows Honeywell to help close the loop within the plastics supply chain by bringing the recycling technology onsite to the collection source. The recycling plants employ a modular design, enabling straightforward deployment and installation, striking the right balance between economy of scale and amount of waste plastic generated locally.

“Our partnership with Honeywell will enable Sacyr to bring sustainable, circular solutions to market,” said Domingo Jiménez, Manager of Sacyr Circular. “The speed with which we can start up plants and the global viability of this solution has the potential to greatly accelerate the impact we can have on the communities we serve, the environment, and society as a whole.”

Honeywell’s UpCycle Process Technology was created within Honeywell’s Sustainable Technology Solutions (STS) group, which is part of Honeywell UOP. This latest technology builds upon Honeywell’s focus to deliver high impact, environmentally sustainable solutions for customers and society.

Honeywell has a long legacy of sustainability-related innovation, including Solstice®, a new generation of low-global-warming-potential hydrofluoroolefin (HFO) refrigerants, aerosols, solvents and blowing agents that can reduce the greenhouse gas emissions impact of current offerings on the market by more than 99 percent. The company also pioneered Ecofining™, a process that converts non-edible natural oils, animal fats and other waste feedstocks to Honeywell Green Diesel™, which is chemically identical to petroleum-based diesel.

 

Honeywell recently committed to achieve carbon neutrality in its operations and facilities by 2035. This commitment builds on the company’s track record of sharply reducing the greenhouse gas intensity of its operations and facilities as well as its decades-long history of innovation to help its customers meet their environmental and social goals. About half of Honeywell’s new product introduction research and development investment is directed toward products that improve environmental and social outcomes for customers.

About Honeywell

Honeywell (www.honeywell.com) is a Fortune 100 technology company that delivers industry-specific solutions that include aerospace products and services; control technologies for buildings and industry; and performance materials globally. Our technologies help everything from aircraft, buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable. For more news and information on Honeywell, please visit www.honeywell.com/newsroom.

  1. The actual utilization rate will depend on a number of factors, such as favorable legislation, status of sorting infrastructure, outcome of LCAs etc.
  2. Honeywell Life Cycle Analysis, October 2021. The LCA results are calculated by Honeywell UOP in accordance with international standards for life cycle assessment, ISO 14040:2006 and 14044:2006. The LCA is pending critical review.
  3. Plastic Energy LCA report: LIFE CYCLE ASSESSMENT OF PLASTIC ENERGY TECHNOLOGY FOR THE CHEMICAL RECYCLING OF MIXED PLASTIC WASTE
  4. BASF LCA report: Evaluation of pyrolysis with LCA – 3 case studies

# # #

Honeywell media contact:

Mike Hockey

(832) 285 4933
Mike.hockey@honeywell.comTehani.manochio@honeywell.com